Search FAQs
Can we use a low voltage current transformer for a medium voltage application?
If the CT will be installed directly on medium voltage busbars, accordingly it must have an insulation level at least equal to that of the system/cubicle. However, if install a toroidal CT will be installed on the medium voltage cable (which is already insulated), in this case the CT can be a low voltage type (e.g. insulated 0.72kV).
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: