{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an APF fault on the ATV61 drive?

Article available in these languages: Spanish

Issue:
APF fault on the ATV61 drive

Product Line:
Altivar ATV61

Environment:
All with an CIC or controller inside card

Cause:
The drive will ramp up and then trip on APF fault.

Resolution:
The APF fault is a fault or error on the controller inside option card.  Try swapping or replacing the controller inside card that has an identical program inside the card.

Schneider Electric Nigeria

Attachment(s)
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]