{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Archive database upgrade fails in database manager

Issue
ION_Data Archive database upgrade fails in PME using database manager

Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x


Environment
Database Manager

Cause
User has ION_Data archive that was created from previous versions of the software and may have been copied and moved to location on external or network drive. Before this archive can be used in PME it must be attached to SQL server with Database Manager and upgraded.

Resolution
Attaching the ION_Data archive database may fail with the following error message: Attached database failed for server .


When you click OK to the error dialog box and try attaching the second time, a new error will reveal more information that will be helpful.


The file permissions changed when the archive database was copied or moved to different locations. To resolve this issue change the permissions to allow "Full control" for the user.
  1. Right clicking on the archive database file (.mdf) and select ->Properties->Security Tab -> Edit button.
  2. Click the add button and add the current user
  3. Select the new user and check the box under Allow for the row "Full control"

Repeat this procedure for the archive Log file (.ldf).

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: