Search FAQs
%MW49..53 seem to be in UTC, how can I get the local time ?
In M580, the words %MW49..53 are in UTC (Coordinated Universal Time), and not in local time.
If local time is needed, use the function RRTC_DT
(note that RRTC_DT_MS is also in UTC time)
If local time is needed, use the function RRTC_DT
(note that RRTC_DT_MS is also in UTC time)
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: