{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I use Cat 6 cables to extend NetBotz sensors with RJ45 connectors?

Issue:

Cat 6 cables do not work when extending NetBotz sensors.

Product Line:

NetBotz

Environment:

NetBotz version 3 sensors with RJ45 connectors

Cause:

Many NetBotz sensors come with a cat5 coupler that enables the RJ45 connection to be extended to an extra 100 feet in most cases (see sensor specs for detail). It has been seen when using cat6 cables instead of cat5 for the purpose of extending the sensor cable, the sensor is unable to be detected.

Resolution:

Due to the differences between cat5 and cat6 cables, please use only cat5 to extend NetBotz sensors.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: