{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Is Small-Load or No-Motor Operation Possible on Altistart 22?
Issue:
Is it possible to run an ATS22 with a smaller motor or without a motor attached?

Product Line:
Altistart ATS22

Environment:
All models

Cause:
Need for testing starter with minimal or no load attached.

Resolution:
No.  SSt is a feature of the ATS48 soft start.  It is not available on the ATS22.
It has to have a load at the output.

The following video is a tutorial for understanding the Small-Load or No-Motor limitations of Altistart 22:

Schneider Electric Nigeria