Issue:
ATV212 OH code (Drive Overtemperature).
Product Line:
All ATV212
Environment:
Any
Cause:
Drive trips on OH:
• The drive cooling fan is not working.
• The ambient temperature is too high.
• An enclosure air vent is blocked.
• A heat source is too close to the drive.
• The drive heatsink temperature sensor is malfunctioning.
Resolution:
• Restart operation by resetting the drive detected fault after cool-off.
• Decrease the ambient temperature by increasing the free space around the drive and removing any heat generating source from the proximity of the drive.
• Check the fan operation