{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I order NEMA style contactors with Enclosed ATS48 soft starts?
Issue:
Order NEMA style contactors for the Enclosed ATS48 soft starts.

Product line:
Enclosed ATS48, Class 8639, Type 48U.

Environment:
All

Cause:
Option not shown in the Product Selector tool.

Resolution:
You must choose Mod W10 which includes  NEMA Style contactors   Please note this option is not available on the Power Circuit R reversing or Mod A10 full voltage bypass option.

Schneider Electric Nigeria

Attachment(s)
30072-450-62_02.pdf [1.93 MB]