{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Why am I getting ": "Warning, application has halted due to : cannot find empty slot to insert error message file KAOScore.txt KAOScore:portable.error.cpp : line 221" and how to resolve the issue?

Issue:
Why am I getting ": "Warning, application has halted due to : cannot find empty slot to insert error message file KAOScore.txt KAOScore:portable.error.cpp : line 221" and how to resolve the issue?

Product Line:
Vijeo Designer

Resolution:
This error is essentially related to the low level error handling system of Vijeo Designer Runtime.
KAOScore.txt is one of several files containing error messages. When an error occurs, Runtime inserts this file into a buffer in order to load the error message.

The error reported occurs when this buffer has somehow become full and Runtime cannot insert any more files.
In theory, this should not happen because there are more slots than there are files.

If there is an ERRORLOG.txt file in the customer's target, it might give us more information as to how the buffer ran out of slots.

But rebooting the target cleans out the buffer and will boot up back to normal. If this does not work, please uninstall and re-install the runtime and reload the program file.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: