undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between the VW3A3310 and the VW3A3310D Modbus Ethernet TCP/IP option cards?
Issue:
VW3A3310 with a "D" on the end of the part number.

Product Line:
ATV71 and ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
The "D" on the end of the VW3A3310D indicates it is equipped for daisy chain and has dual RJ45 connectors.  A network cable can go into one RJ45 and out the other to connect to the next drive in the network.  The VW3A3310 has only one RJ45 port.

Schneider Electric Nigeria