{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Cannot transfer the Unity application to the PLC after updating the M580 exec firmware.
Issue
Cannot transfer the Unity application to the PLC after updating the M580 exec firmware.

Product Line
M580

Product Line
Unity Pro v13.1, Windows 10 version 1902, BMEP583040 v2.70

Resolution
If you try to transfer an application to an M580 after performing an update of the exec firmware, the 'Transfer Project to PLC' selection in Unity could be greyed out and unselectable.
fdfrf

If you try to shutdown Unity and restart the software, it may not resolve the issue.

To resolve the issue, the PC will need to be rebooted.

This could happen if Unity has been connected to the PLC and disconnected from the PLC multiple times prior to updating the exec firmware.



Schneider Electric Nigeria