{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an PTFL fault on the ATV61 and ATV71 drives?
Issue:
PTFL fault on the ATV61 and ATV71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Drive is faulting on power up.

Resolution:
This is a PTC error fault.   Check to see if the PTC switch is turned ON if so check to see if the PTC input is open or shorted.

Schneider Electric Nigeria