{}

Our Brands

Impact-Company-Logo-English Black-01-177x54
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Search FAQs
PowerChute Network Shutdown reports "Available runtime has been exceeded".

Article available in these languages: Spanish

Issue:
PowerChute Network Shutdown reports "Available runtime has been exceeded". and or PowerChute shuts down OS due to "Available runtime has been exceeded"

Product:
PowerChute Network Shutdown versions 4.x, 5.x

Environment:
All supported OS
NOTE: All of this information is available in the User Guides and PowerChute Help.

Cause:
Condition 1 for all configurations except VMware and Hyper-V:
When the total shutdown time required by PowerChute is greater than the Low Battery Duration minus two minutes configured for the UPS. In the event of a low battery condition, PowerChute will not have enough time to complete the shutdown sequence before the UPS powers off. For example, if the total shutdown time required is 3 minutes and Low Battery Duration is 4 minutes, the Available Runtime has been Exceeded event will be triggered.

Condition 2 for all configurations except VMware and Hyper-V:
When the shutdown duration configured for the UPS On Battery event plus the total shutdown time required by PowerChute is greater than the Runtime Remaining on the UPS minus two minutes. This condition can be caused by having a load that is too great on the UPS when the battery is fully charged.

Condition 3 and 4 are for VMware configurations.
For  conditions 3 and 4 below, the "total shutdown time" includes the following durations:

  • VM migration duration
  • VM shutdown and startup duration
  • vApp shutdown and startup duration
  • vCenter Server VM shutdown duration
  • Disable vCLS duration
  • Disable HA duration
  • AFS shutdown and startup duration - Nutanix only
  • Abort Active Replications duration - Nutanix only
  • Cluster shutdown and startup duration - Nutanix, HyperFlex, and Dell VxRail only
  • Controller VM shutdown and startup duration - Nutanix and HyperFlex only
  • OVC shutdown and startup duration - SimpliVity only
  • Maintenance mode duration for Dell VxRail stretched cluster
  • Shutdown command file duration
  • SSH action duration
  • Built-in duration of 2 minutes (this consists of a 10-second OS shutdown duration and a 60 second OS shutdown duration; rounded up)

The event occurs with either of the following conditions:

Condition 3 for VMware:
When the total shutdown time required by PowerChute is greater than the Low Battery Duration minus two minutes configured for the UPS. In the event of a low battery condition, PowerChute will not have enough time to complete the shutdown sequence before the UPS powers off. For example, if the total shutdown time required is 3 minutes and Low Battery Duration is 4 minutes, the Available Runtime has been Exceeded event will be triggered.

Condition 4 for VMware:
When the shutdown duration configured for the UPS On Battery event plus the total shutdown time required by PowerChute is greater than the Runtime Remaining on the UPS minus two minutes. This condition can be caused by having too great a load on the UPS when the battery is fully charged.

Condition 5 and 6 are for Microsoft Hyper-V configurations.
For conditions 5 and 6 below, the "total shutdown time" includes the following durations:

  • VM migration duration - Hyper-V only
  • VM shutdown and startup duration- Hyper-V only
  • Host Maintenance duration - SCVMM only
  • Shutdown command file duration
  • SSH action duration
  • Built-in duration of 2 minutes (this consists of a 10 second OS shutdown duration and a 60 second OS shutdown duration; rounded up)

The event occurs with either of the following conditions:

Condition 5 for Hyper-V:
When the total shutdown time required by PowerChute is greater than the Low Battery Duration minus two minutes configured for the UPS. In the event of a low battery condition, PowerChute will not have enough time to complete the shutdown sequence before the UPS powers off. For example, if the total shutdown time required is 3 minutes and Low Battery Duration is 4 minutes, the Available Runtime has been Exceeded event will be triggered.

Condition 6 for Hyper-V:
When the shutdown duration configured for the UPS On Battery event plus the total shutdown time required by PowerChute is greater than the Runtime Remaining on the UPS minus two minutes. This condition can be caused by having too great a load on the UPS when the battery is fully charged.

Solution:

Condition 1 for all configurations except VMware and Hyper-V:
Increase the Low Battery Duration value on the NMC using Configure - Shutdown or decrease the shutdown durations being used by PowerChute.

Condition 2 for all configurations except VMware and Hyper-V:

  1. Remove some equipment from the UPS to increase the available runtime.
  2. Decrease the shutdown duration time for the UPS On Battery event.
  3. Decrease the command file execution time using the Shutdown Settings screen.

This event is logged and event actions are carried out even if it occurs on a single UPS in a
Redundant or Parallel UPS configuration.

Condition 3 for VMware:
Increase the Low Battery Duration value on the NMC using Configure - Shutdown or decrease the shutdown durations being used by PowerChute.

Condition 4 for VMware:

  1. Remove some equipment from the UPS to increase the available runtime.
  2. Decrease the shutdown duration time for the UPS On Battery event.
  3. Decrease the command file execution time using the Shutdown Settings screen.

This event is logged and event actions are carried out even if it occurs on a single UPS in a Redundant or Parallel UPS configuration.

Condition 5 for Hyper-V:
Increase the Low Battery Duration value on the NMC using Configure - Shutdown or decrease the shutdown durations being used by PowerChute.

Condition 6 for Hyper-V:

  1. Remove some equipment from the UPS to increase the available runtime.
  2. Decrease the shutdown duration time for the UPS On Battery event.
  3. Decrease the command file execution time using the Shutdown Settings screen.

This event is logged and event actions are carried out even if it occurs on a single UPS in a Redundant or Parallel UPS configuration.

Schneider Electric Nigeria

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.