{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can a psx file from Somove be converted to a cfg Multiloader file?

Issue:
SoMove conversion from PSX to a CFG Multiloader File.

Product Line:
Multiloader, VW3A8121

Environment:
All serial numbers for VW3A8121

Cause:
N/A

Resolution:
In SoMove, click on the Multi-Loader/SoMove Mobile option.
Once it opens, pick your psx file and click Export.
It will export the file as a cfg file which can be saved on an SD card for the Multiloader.
Once the SD card is placed in the Multiloader then the file can be transferred to the drive.

Schneider Electric Nigeria