{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to program a new M340 out of the box via the serial port?
Title
Program a new M340 out of the box via the serial port

Issue
Loading intial program into M340

Product Line
M340

Environment
Unity Pro, Control Expert

Resolution
Yes. By default without a program loaded the serial port of the M340 is set to RS485, Slave mode, 9600, 8, E, 1 and Address#1.
Using the TSXCUSB485 RS485 to USB adapter with a standard Ethernet patch cable connected to the M340 serial port you will be able to connect with Unity Pro to download a project.


**The position of the rotary switch must be set to #0= TER MULTI or #1= OTHER MULTI **


Schneider Electric Nigeria