{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Cannot View diagrams in engineering client after running EPSS Generator tool
Issue
Diagrams created from EPSS generator tool will not open in engineering client , Diagrams open fine in Vista on from the server.

Product Line
PMEHC 7.22
PMEDC 7.22
PME 8, 8.1, 8.2

Environment
StruxureWare Power Monitoring Expert Vista Application

Cause
EPSS Generator tool does not bring the network  path over for the diagrams.  Right clicking on the link in vista will show the local server path for the diagrams "C:\Program files(X86)\Schneider Electric\Power Monitoring Expert\config\diagrams\ud\EPSS\diagram.dmg "

Resolution

1. In Vista engineering client click "File > Open" you will see the server path to the diagrams you can copy this or note it.

2. Right click on the link  in the engineering client and then select the action tab in the path field.

3. Remove the local path EG: "C:\Program files(X86)\Schneider Electric\Power Monitoring Expert\config\diagrams\ud\EPSS\diagram.dmg "  keeping the diagram name and past the server path you copied,  it will now look something like this:
"\\Powerlogic02\ION-Ent\config\diagrams\ud\EPSS\diagram.dgm"

4. You will need to do this for each link created by the generator tool.


Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: