Issue
User wants to import XML data by unable to determine if XML import module has a problem with the XPATH or connecting to the XML data
Product
ION Enterprise
StruxureWare Power Monitoring Expert 7.0, 7.0.1
Power Monitoring Expert 7.2.x, 8.x including Health Care and Data Center editions.
Power Monitoring Expert 9.0, 2020
Environment
Designer
Cause
XML import module does not provide detailed message when unable to locate desired XML information
Resolution
The following link provides a free XPath test application.
XPATH tester
1) Enter the raw XML data in the field "XML Input" or a link to the XML data and the test Xpath for the desired information
2) Click the button "TEST XPATH"
The result with display what information the XPATH is able to retrieve from the XML data or provide an error message.
User wants to import XML data by unable to determine if XML import module has a problem with the XPATH or connecting to the XML data
Product
ION Enterprise
StruxureWare Power Monitoring Expert 7.0, 7.0.1
Power Monitoring Expert 7.2.x, 8.x including Health Care and Data Center editions.
Power Monitoring Expert 9.0, 2020
Environment
Designer
Cause
XML import module does not provide detailed message when unable to locate desired XML information
Resolution
The following link provides a free XPath test application.
XPATH tester
1) Enter the raw XML data in the field "XML Input" or a link to the XML data and the test Xpath for the desired information
2) Click the button "TEST XPATH"
The result with display what information the XPATH is able to retrieve from the XML data or provide an error message.
Released for:Schneider Electric Nigeria