{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
UL listing for a BCPM EM3500, EM4900, MCM and the SMD
Issue
User wants to know where to find the UL listing for the BCPM or the EM3500

Product Line
BCPM, Series BCPMSC*, EM3502, EM3502A, EM3550, EM3550A, EM3555, EM3560, EM3560A, EM3561, EM3561A,EM3570

Resolution
The UL listing for a BCPM EM3500, EM4900, MCM and the SMD are listed as a Power Circuit and Motor-mounted Apparatus which complies with UL standard 508 " Industrial Control Equipment . The UL listing is E191129


USA:
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/showpage.html?name=NMTR.E191129&ccnshorttitle=Power+Circuit+and+Motor-mounted+Apparatus&objid=1079307826&cfgid=1073741824&version=versionless&parent_id=1073990288&sequence=1

Canada:
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/showpage.html?name=NMTR7.E191129&ccnshorttitle=Power+Circuit+and+Motor-mounted+Apparatus+Certified+for+Canada&objid=1079307821&cfgid=1073741824&version=versionless&parent_id=1073990290&sequence=1

Schneider Electric Nigeria