{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the advantage of 750 mm wide cabinets over 800 mm wide cabinets?
Issue:
Customers want to know if there is an advantage of having 750 mm wide cabinets.

Product Line:
NetShelter SX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
Customers need help choosing the correct cabinet width.

Resolution:

In a long row, the 750 mm wide cabinet saves space over the 800 mm wide cabinet.
Sixteen (16) 750 mm wide cabinets can fit into the same space as a (15) 800 mm wide cabinets:
  • 750 mm wide - 16 cabinets = 12.0 meter.
  • 800 mm wide - 15 cabinets = 12.0 meter.

Schneider Electric Nigeria