{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will the VW3G48101 keypad kit for the ATS48 series soft starts work with the ATS46 series soft starts?
Issue:
Can I use the VW3G48101 keypad kit of the ATS48 to connect to the ATS46?

Product Line:
VW3G48101 remote mount keypad kit for use with the ATS48 series starters.

Environment:
All models, All serial numbers.

Cause:
Customer has ATS46 soft starters and needs a remote mount keypad kit.  The kit designed for the ATS46 is obsolete and no longer available.

Resolution:
No.  The VW3G48101 remote mount keypad kit is compatible with ATS48 series soft starters only.  It will not work with the ATS46 series soft starters.

Schneider Electric Nigeria