{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum number of channels of the Modbus TCP IO Scanner of a TM251MESE in Machine Expert or SoMachine?

Article available in these languages: Spanish

The maximum number of the Modbus TCP IO Scanner channels of a TM251MESE is 64 channels.

Examples:
1. One Modbus TCP slave with 64 channels
1. 64 Modbus TCP slaves each with one channel
2. Two Modbus TCP slave each with 32 channels or any combination between the two slaves that does not exceed 64 channels total

This information was verified for Machine Expert 2.0, Machine Expert 1.2, SoMachine 4.3, SoMachine 4.2, SoMachine 4.1

Schneider Electric Nigeria