{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is TCSWAAC13FB Universal Bluetooth Interface supported with Android App to be used with a Mobile phone?
Issue:
Mobile phone and Bluetooth adaptor.

Product Line:
ATV71, ATV61, ATV312, ATV12, ATS48, ATS22

Environment:
All

Cause:
N/A

Resolution:
The TCSWAAC13FB is a Modbus-to-Bluetooth adaptor, used to activate any non-Bluetooth device to communicate via Bluetooth wireless link.
If you want to configure the ATV drive from your phone, you need to install SoMove Mobile into your telephone.
However, it can only support Symbian or Blackberry mobile. It does not support Android or iOS operating systems.

Schneider Electric Nigeria