{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
BMXFTW308S cable diameter
Issue
This Resolution explains the maximum diameter for the BMXFTW308S cable.



Product Line
BMXFTW308S



Resolution
The cable diameter is 11.2mm.


The BMXFTW308S cable is a shielded cable used with  the M340 I/O modules.
It has a 28 pin terminal block on one end and color-coded flying leads on the other end.





Schneider Electric Nigeria