{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Token ring topology with Modbus Ethernet TCP/IP.
Issue:
Can the ATV32 drive with Modbus Ethernet TCP/IP do token ring topology?

Product Line:
ATV32

Environment:
All models and serial numbers

Cause:
None

Resolution:
No, the token ring topology is not compatible with the ATV32 running Modbus Ethernet TCP/IP protocol.   See the Modbus TCP Ethernet/IP Communication Manual S1A28701 for further details.

Schneider Electric Nigeria

Attachment(s)
atv32_modbus_tcp_ethernet_ip_manual_s1a28701_02.pdf [9.44 MB]