{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I assign a different logic input other than LI1/DI1 to run forward on an Altivar drive?

Article available in these languages: Spanish

Issue:
Set logic inputs other than LI1/DI1 for run forward command on an Altivar drive.

Product Line:
Altivar drives

Environment:
All

Cause :
LI1 logic input inoperative

Resolution:
In 2 wire control, LI1/DI1 is run forward. In 3 wire control, LI1/DI1 is stop and LI2/DI2 is run forward.
In either configuration, LI/DI1 must be active for the drive to run and no other inputs can be assigned as run forward.


Schneider Electric Nigeria