{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to add a 170ADO83030 Momentum I/O Base to the Unity Catalog
Issue
This Resolution explains how to add a Momentum I/O base to the pick list in Unity Pro Software versions 8.0 and higher.


Some older Momentum I/O bases were not supported in Unity.  Support for these modules can be added by using the Unity Hardware Catalog Manager along with the module CPX file, which will be imported into Unity and added to the pick list.


Product Line
170ADO83030



Environment
Unity Pro V8 and higher


Resolution
There are two files attached to this resolution.
  • The file, 'Adding IO Bases to the Unity Catalog.pptx', is the procedure to import the CPX file.
  • The file, ADO83030.cpx, is the file that will be imported into Unity.  (unzip file 'ADO83030 cpx file.7z)

When the import is completed, the module will show up in the picklist as follows:


Schneider Electric Nigeria

Attachment(s)
ADO83030 cpx file.7z [3.38 KB]
Adding IO Bases to the Unity Catalog.pptx [115.78 KB]