{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How I can use the Profibus module TM4PDPS1 with the Modicon TM241
When you use the module Profibus TM4PDPS1 with the PLC TM241xx, is mandatory to use:

-A dedicated PROFIBUS task configured without watchdog (Do not use the MAST)

-The dedicated PROFIBUS task MUST have a lower priority than the MAST task. ex: if the MAST task has a priority value 1, so the TaskProfibus needs to have a priority value 10.
-Do not set the PROFIBUS task cycle time faster than 10 ms.

Schneider Electric Nigeria