{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can Vijeo Designer simulator communication out of the serial port to a controller over serial?
Issue:
Can Vijeo Designer simulator communication out of the serial port to a controller over serial?

Product Line:
Vijeo Designer

Resolution:
Yes, but the Vijeo Designer simulator will only communicate on the PC native COM1 serial port.  It will not communicate over the USB to serial converters.

Schneider Electric Nigeria