Search FAQs
Which Windows operating systems are compatible with the new MBX v8.1 driver suite.
The new MBX v8.1 driver suite is compatible with the following Windows operating systems:
* 64-bit Windows operating systems do not support Virtual MBX Driver technology. However, Cyberlogic has provided support for the operation of the Virtual MBX Driver in 64-bit operating systems using 32-bit Windows XP under Virtual PCs, if enabled by the 64-bit operating system.
MBX Component | MBX Driver | Virtual MBX Driver | MBX Gateway Driver | Ethernet MBX Driver |
Windows 8 (32 bits) | x | x | x | x |
Windows 8 (64 bits) | x | * | x | x |
Windows 7 (32 bits) | x | x | x | x |
Windows 7 (64 bits) | x | * | x | x |
Windows Vista (32 bits) | x | x | x | x |
Windows Vista (64 bits) | x | * | x | x |
Windows XP (32 bits) | x | x | x | x |
Windows XP (64 bits) | x | * | x | x |
Windows Server 2012 (32 bits) | x | x | x | x |
Windows Server 2012 (64 bits) | x | * | x | x |
Windows Server 2008 (32 bits) | x | x | x | x |
Windows Server 2008 (64 bits) | x | * | x | x |
Windows Server 2003 (32 bits) | x | x | x | x |
Windows Server 2003 (64 bits) | x | * | x | x |
* 64-bit Windows operating systems do not support Virtual MBX Driver technology. However, Cyberlogic has provided support for the operation of the Virtual MBX Driver in 64-bit operating systems using 32-bit Windows XP under Virtual PCs, if enabled by the 64-bit operating system.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: