{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the NetShelter SX Networking cabinets available in a Shock Package version?
Issue:
None of the Networking cabinets have Shock Package versions.

Product Line:
NetShelter Networking

Environment:
All versions and serial ranges.

Cause:
A request has been made for Networking cabinets to be able to ship with equipment installed.

Resolution:
No, the NetShelter SX Networking cabinets are not available in Shock Package versions. The NetShelter Networking cabinets have mounting rails that are open to allow greater airflow. This design has not been tested for shock packaging.

Schneider Electric Nigeria