{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What cable is recommended to be used with the VW3A1006 remote keypad?

Issue:
Cable recommendation to be used with the VW3A1006 remote keypad

Product Line:
Altivar ATV12 ATV32

Environment:
All

Cause:
Wants to know what cable is recommended for the VW3A1006 keypad display.

Resolution:
Cable that has part number as VW3A1104R10 (1m) or VW3A1104R30(3m) can be used.

Schneider Electric Nigeria

Attachment(s)

Untitled.pngUntitled.png [70.35 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: