{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert 7.2.2/8.0 - User is seeing many system log errors from xl20 after they upgraded from ION Enterprise to PME
Issue
Power Monitoring Expert 7.2.2/8.0 - Why is user seeing so many system log errors from xl20 after they upgraded from ION Enterprise to PME?

Product Line
PME7, PME7.2, PME8.0

Environment
Device Communications

Cause

When ION Enterprise systems that include 3720 ACM devices are upgraded to Power Monitoring Expert 7.2.2, it is possible that the system log will be flooded with errors like:

An unknown exception occurred in XL20
Transaction error. Device: 'LVPML2.D148_Tie_To_J103'. Client: 'IONSERVICES.WALONAION12'. Reason: 'VSIN_MessageUndefined'
Transaction error. Device: 'LVPML2.B16_PACLAM'. Client: 'IONSERVICES.WALONAION12'. Reason: 'VSIN_PasswordLenErr'
Transaction error. Device: 'LVPML2.B16_PACLAM'. Client: 'IONSERVICES.WALONAION12'. Reason: 'VSIN_UnderflowStream'

These errors are typically only nuisance errors, but there can be many of them. There have been some cases where the Site Server service crashes as a result of these errors.

Resolution
This can be corrected by applying the attached xl20.dll patch.

*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).
To deploy:
1. Shut down the ION Site Server service
2. Rename the existing file \system\bin\xl20.dll
3. Copy in the attached file
4. Restart the ION Site Server service

NOTE: The patch for PME 7.2.2 is different then PME 8.0 patch. Be sure to match the patch to the software version.

Schneider Electric Nigeria

Attachment(s)
PME722_Hotfix_46202_xl20.7z [255.74 KB]
PME8_Hotfix_46202-xl20.zip [363.59 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.