Issue:
Max speed above 60Hz on Altivar 12
Product line:
Altivar 12, ATV12
Environment:
All
Cause:
N/A
Resolution:
From main display of RDY, push the enter button (dial) and turn the dial to CONF. Push enter and then scroll to FULL. Push enter and scroll down to DRC. Push enter and scroll down to TFR.
When the drive is initially setup as 60Hz, the TFR changes to 72 by default. Increase TFR to the max frequency you want to be able to run the motor at. Push Enter to save.
Escape back until you see FULL. Then scroll up to HSP. Push enter and change the High speed to the maximum speed you want the drive to run. The analog signal by default will follow LSP to HSP values.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Nigeria