undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What cable is used to communicate via Modbus TCP/IP (USB Equipment) between the M340 to HMIGTO?
Issue:
Looking for assistance on how to connect the M340 PLC to a Magelis HMI in order to communicate over Modbus TCP/IP USB Equipment as defined in Vijeo Designer.

Product Line:
Vijeo Designer, Magelis HMI, M340 

Resolution:
The BMX-XCA-USBH018 is the cable to communicate by Modbus TCP/IP via USB between the M340 and the HMIGTO5310.

The mini-USB end plugs into the M340 and the standard USB end plugs into the HMIGTO

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.