{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
IEC61850 documentation for VAMP
Issue
Need to program the VAMP relay with the IEC61850 communication.

Product Line
VAMP 5x, 2xx, 3xx

Environment
VAMP set and SCD Editor

Resolution
Attached are the manuals for programming the VAMP for IEC61850

​Latest information is available in m.vamp.fi

Schneider Electric Nigeria

Attachment(s)
AN61850.EN002 IEC 61850 interface configuration for VAMP relays.pdf [664.75 KB]
VM61850RELAYSCON.EN002.pdf [777.83 KB]