{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Data Center Expert | How do I configure auto-login when launching to APC devices?
Issue:
How do I configure auto-login when launching to APC devices within the StruxureWare Data Center Expert desktop client?

Product Line
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)

Environment
StruxureWare Data Center Expert (all versions)
StruxureWare Central (all versions)
InfraStruXure Central (all versions)

Cause:
Double clicking on an APC device (NMC) in StruxureWare DCE launches a browser window to that device automatically logging in if configured correctly.

Resolution:



1) Open the DCE desktop client and navigate to: Monitoring perspective > Device View pane.
2) Right-click on an APC device and select Device Launch settings. Use Ctrl+click or Shift+click to select multiple devices at once.
3) Ensure that the correct protocol, port, username, and password are defined for accessing the devices web interface.  Select OK.
4) Double-click on the device, or right-click and select Launch to Device, and the web interface of the device should load and automatically log in.

Schneider Electric Nigeria