What is the replacement for the Magelis XBTG5330 HMI?
The Magelis XBTG5330 HMI was replaced by the XBTGT5330. However, the end of commercialization for the Magelis XBTGT5330 HMI was on June 30, 2015. The XBTGT5330 can be replaced by the HMIGTO5310.
Released for:Schneider Electric Nigeria
Explore more
Range:
Magelis XBT GT
Harmony GTO
Magelis XBT GC
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.