{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
On the I/O are they listed as digital. What kind? Encoder? 0-10V? or just on or off.
Inputs are designed to be connected to a potential free contact. Be carefully that there are several types of inputs: - safety inputs, limit switches inputs and alarm inputs. This wiring diagram is depending on the input function.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.