{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Degree of Protection (IP) of an external protection enclosure for a TRIHAL Cast Resin dry type transformers?
For indoors, the standard protection enclosure of the TRIHAL cast resin dry type transformer is IP 31. For non-standard and indoors, an IP 23 enclosure for a polluted atmosphere can be installed. For outdoors and customised transformers, an IP 35 minimum protection enclosure can be ordered.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.