{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the recommended value for hours of operating a Trihal cast resin dry type transformer 2000 Kva AN/AF in forced ventilation ?
The forced ventilation option is a ''customized''solution that must be detailed on ordering phase in TRIHAL cast resin dry type transformer,also we believe that using the option of forced ventilation can be applied all along the day but with much reduced transformer service life(can be short as 3.5 years comparing to 30 years without ventilation.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.