What is the thermal class insulation for Tricast cast resin dry type transformers?In standard, the thermal insulation class is Class F for Tricast cast resin dry type transformers. Also Class H can also be provided as an option.
Released for:Schneider Electric Nigeria