{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Index issue due after conversion from Modsfoft, Proworx or Concept application in Unity Pro.
In Unity pro Index can be :
  • a value belonging to an Integer type
  • an arithmetical expression made up of Integer types
But cannot contain an other indexed variable, in this case a tempory variable will have to be created and used .

Example :
SortInterfaceOut.SortLQuantity := Decode_Pallet_Pattern[Scanner_Info[8].PIF.Pattern].CasesPerPallet;
is converted to this code by Unity pro : SortInterfaceOut.SortLQuantity := Decode_Pallet_Pattern[Scanner_InfoDecode_Pallet_PatternsPerPallet;

In order to avoid this, just affect in a temporary variable the value of "Scanner_Info[8].PIF.Pattern" :
Temp_Int := Scanner_Info[8].PIF.Pattern;
SortInterfaceOut.SortLQuantity := Decode_Pallet_Pattern[Temp_Int].CasesPerPallet;

Schneider Electric Nigeria