Search FAQs
Where to reconfigure, in BLAT, the SMTP server parameter
Issue
BLAT is configured on server to send out email using the Launching Module in VIP. The SMTP server has changed and need to reconfigure in BLAT.
Product Line
SPM7.x
PME7.x
Power Monitoring Expert (PME 8.x)
Environment
Windows
Cause
BLAT is configured on server to send out emails using the Launching Module in VIP. The SMTP server has changed and need to reconfigure BLAT
Resolution
When BLAT was configured on the server the install command only stores the various parameters in the Windows Registry. To change or verify the SMTP settings navigate to Regedit ->HKEY_LOCAL_MACHINE ->SOFTWARE ->Wow6432Node ->Public Domain ->Blat. The configured parameters that BLAT uses can be found here.
BLAT is configured on server to send out email using the Launching Module in VIP. The SMTP server has changed and need to reconfigure in BLAT.
Product Line
SPM7.x
PME7.x
Power Monitoring Expert (PME 8.x)
Environment
Windows
Cause
BLAT is configured on server to send out emails using the Launching Module in VIP. The SMTP server has changed and need to reconfigure BLAT
Resolution
When BLAT was configured on the server the install command only stores the various parameters in the Windows Registry. To change or verify the SMTP settings navigate to Regedit ->HKEY_LOCAL_MACHINE ->SOFTWARE ->Wow6432Node ->Public Domain ->Blat. The configured parameters that BLAT uses can be found here.
Released for:Schneider Electric Nigeria
Explore more
Product:
Explore more
Product: