{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you use the ATS22 Soft Starter on an open delta system?

Article available in these languages: Spanish

Issue:
ATS22 soft starter on an open delta system

Product Line:
Altistarter ATS22 and 22U

Environment:
All

Cause:
Wants to use the ATS22 on an open delta system.

Resolution:
There is nothing published that says you cannot use the ATS22 soft starters on an open delta system. If the phase to phase voltages are balanced, it should be ok.

Schneider Electric Nigeria