Issue:
Programming the ATV312 to run without the motor connected.
Product Line:
ATV312 drives
Environment:
Run the drive without a motor connected
Cause:
ATV312- needs to run the drive without a motor connected
Resolution:
Suggested to go to FLT menu: set OPL to no.
Then can run the drive open circuit.
Programming the ATV312 to run without the motor connected.
Product Line:
ATV312 drives
Environment:
Run the drive without a motor connected
Cause:
ATV312- needs to run the drive without a motor connected
Resolution:
Suggested to go to FLT menu: set OPL to no.
Then can run the drive open circuit.
Released for:Schneider Electric Nigeria