Issue
Modicon M580 support for Quantum ERIO drops
Product Line
Modicon M580 PAC, Quantum
Resolution
The Modicon M580 models BMEx584040, 5040 and 6040 will support Quantum ERIO drops when used with Unity 11.0 running Hot Fix 1 or later. Hot Fix 1 will also allow State RAM addressing for the Quantum ERIO drop.
Modicon M580 support for Quantum ERIO drops
Product Line
Modicon M580 PAC, Quantum
Resolution
The Modicon M580 models BMEx584040, 5040 and 6040 will support Quantum ERIO drops when used with Unity 11.0 running Hot Fix 1 or later. Hot Fix 1 will also allow State RAM addressing for the Quantum ERIO drop.
Released for:Schneider Electric Nigeria