{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the range of the nCr parameter on the ATV312 series drive?
Issue:
Programming range for the nCr (Nominal Current) Parameter

Product Line:
ATV312 series drives

Environment:

All models, All serial numbers

Cause:
Information needed for pre-purchase product selection.

Resolution:
The nCr (motor current rating) parameter can be adjusted between 25% and 150% of the nominal rating of the drive, as listed on the drive nameplate.

Schneider Electric Nigeria