{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can AR8008BLK or AR8016ABLK be used in the NetShelter Networking cabinets?
Issue:
The NetShelter SX Networking cabinets have open mounting rails which do not support the cable side channels.

Product Line:
NetShelter SX Networking

Environment:
All versions and serial ranges.

Cause:
A customer needs to run cables from front to rear in a NetShelter SX Networking cabinet.

Resolution:
In the Networking cabinets horizontal cable managers can be used to connect the side channels from front to rear. A typical setup would be to have AR8603A or AR8428 installed on the front and rear mounting rails, and run AR8008BLK or AR8016ABLK between them.

Schneider Electric Nigeria