Search FAQs
Which port will L9_XMIT function block work with on the Unity 140CPU31110?
Issue
The Unity help does not state which ports on the 140CPU31110 supports the L9_XMIT function block.
Product Line
Ecostruxure Control Expert (formerly known as Unity Pro), Quantum
Environment
Unity Pro v10, 140CPU31110
Resolution
The Unity documentation shows the following statement for the XMIT block.but it does not specify the PLC
type. The Unity 140CPU31110 only has two Modbus ports.
Function Description
The L9_XMIT (transmit) function block sends Modbus messages from a master PLC to multiple slave PLCs or
sends ASCII character strings from the PLC's Modbus slave port #0, port#1, or port#2 to ASCII printers and
terminals. L9_XMIT sends these messages over telephone dial up modems, radio modems, or simply direct
connection.
The L9_XMIT will only work with Modbus port 1 on the 140CPU31110.
The Unity help does not state which ports on the 140CPU31110 supports the L9_XMIT function block.
Product Line
Ecostruxure Control Expert (formerly known as Unity Pro), Quantum
Environment
Unity Pro v10, 140CPU31110
Resolution
The Unity documentation shows the following statement for the XMIT block.but it does not specify the PLC
type. The Unity 140CPU31110 only has two Modbus ports.
Function Description
The L9_XMIT (transmit) function block sends Modbus messages from a master PLC to multiple slave PLCs or
sends ASCII character strings from the PLC's Modbus slave port #0, port#1, or port#2 to ASCII printers and
terminals. L9_XMIT sends these messages over telephone dial up modems, radio modems, or simply direct
connection.
The L9_XMIT will only work with Modbus port 1 on the 140CPU31110.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: