{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which port will L9_XMIT function block work with on the 171CBUxxxxx Unity Momentum
Issue
The Unity help does not state which ports on the 171CBUxxxxx Unity Momentum supports the L9_XMIT function block.

Product Line
EcoStruxure Control Expert (formerly known as Unity Pro), Unity Momentum

Environment
Unity Pro v10, 171CBU98090

Resolution
The Unity documentation shows the following statement for the XMIT block, but it does not specify the PLC
type. The Unity Momentum only has two Modbus ports but they are labeled as port 1 and 2.

Function Description
The L9_XMIT (transmit) function block sends Modbus messages from a master PLC to multiple slave PLCs or
sends ASCII character strings from the PLC's Modbus slave port #0, port#1, or port#2 to ASCII printers and
terminals. L9_XMIT sends these messages over telephone dial up modems, radio modems, or simply direct
connection.

The L9_XMIT will only work with both Modbus port 1 and 2 on the 171CBUxxxxx Unity Momentum PLC. In order for
it to work, the L9_XMIT will have to be configured for port 0 if you want to use Modbus port 1 and port 1 if you want
to use Modbus port 2.

Schneider Electric Nigeria